Note: This feature is available only for power meters and power sensors that support trace charts shown in the Trace display view.
The Gate function allows you to apply a gate on the trace chart to determine the values of the various pulse waveform parameters. Two vertical limit lines are placed on the Trace chart to mark the boundary of the gate. The application supports up to four gates in a graph. You can also use this feature together with Markers.
The following Gate pulse measurement parameters are supported:

Select your desired parameters and click "X" to close the dialog. Your selected parameters will now be added to the Pulse Analysis table (see example below).
To remove a specific parameter from the Pulse Analysis table, select a row and click the "Remove Row" button. To clear the entire table, click the "Remove All Rows" button.
Power Measurements Using Trace View